Other Parts Discussed in Thread: TLV272,
Hi all ,
I am using the TMCS1101A2BQDR IC in our 3 Phase Inverter for motor control application for phase current sensing. I am facing an issue regarding the IC power on time. I have observed a varying delay time between the instant the IC supply voltage appears to the instant the IC offset voltage appears at the IC output terminals. In the datasheet it was mentioned the power on time as 25msec but I am observing a variable delay time with maximum of 3 seconds. In the image uploaded one can see a delay of 1second. Blue is the IC supply voltage and Pink is the IC output voltage. Can someone through some light on why exactly this is happening
Fig 1 : Delay of 1 second between Vcc(Blue) and Vo (Pink)
The IC output is driving one of the channels of the 2 channel opamp IC TLV272. I have removed the connection between these two ICs but still the issue persists. The issue is not consistent, sometimes there is only 25msec delay between the IC supply voltage and IC output like it was mentioned in the datasheet.
Fig 2 : Delay of 25msec (matching with datasheet ) between Vcc ( Blue) and Vo( Pink)