This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to modify the interference Lab to detect the fixed frequency of the interferer radar



Hi,

In the Interference Mitigation and Detection Lab, there are two radar devices, one is the interferer radar which sending a continuous and fixed frequency, another is the victim normal radar.

I want to detect the spectrum of the interferer radar firstly. It can be achieved by keeping the RXs active and the TXs switched off, and then perform FFT for the recieved ADC data. How can I modify the lab source code to achieve the function? Thanks.