Part Number: TMCS1100
Hi,
in the Datasheet as well as in the product folder it say's for the TMCS1100 and TMCS1001 that it will work for 5V and 3.3V with even a min. spec of 3.0V Vcc. When although lookign to the tables inside the Datasheets there is the issue that for the A4 versions with 400mV/A gain this seems the 3.3V optins are not supported becaus its "--"
Could you explain if the devices will still work down to 3.0V ?
If yes are there any spec's which can not be met anymore?
If no what is the min Vcc the A4 Versions would work and what is the gating item ?
Thanks alot, Bertram