Let's suppose I have enabled two different transmit antennas. I would like to transmit Chirp 1, with starting frequency F1, slope K1, and phase offset P1 using Tx Antenna 1, while simultaneously transmitting Chirp 2 with starting frequency F2, slope K2, and phase offset P2 using Tx Antenna 2. Is this possible?
The TI documentation shows the following:
So it is clear I could enable Tx1 to transmit Chirp 1 during Burst 1 and then Tx2 to transmit Chirp 2 during Burst 2. However, is it possible to do this simultaneously, i.e. to use two different transmit antennas with different chirp configurations within a single burst?
If it is possible, could you help me with the commands necessary to configure the IWR6843 to do this?
Thanks :-)