This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Measuring optical signals near the detection limit

Part Number: OPT3002
Other Parts Discussed in Thread: OPT3001, OPT3002

Hello,

I’m using the OPT3001 in a optical scattering system to measure non-specular reflectance from smooth surfaces. The detected light is near the detection limit 1.2nW/cm-2. My calculations are showing a non-linear response at these levels of optical input. Please provide data showing the linear response of this device throughout its operating range. I know that it uses a log amp to measure across the 7 orders of magnitude of the Silicon response, but I’m hoping that the reported irradiance values are indeed correct even at low light levels.

Thank you,

Patrick

  • Hello Patrick,

    I want to quickly make sure you are using the OPT3001 and not the OPT3002.  I am assuming the OPT3002 is being used as yo you referenced the measurement level.  The figures in section 6.7 show the response of the OPT3002 across temperature range, supply voltage, incidence angle, and input illuminance.

    Rahland