This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sensors, raw12, has mipi signal in the output of Deserializer, but can't be captured by tda4, Deserializer 96722 Serializer 96705

Hi! TI's experts!

    We can't make the 0147 sensors work in tda4! 

    There are 4 same cameras, without isp, 1280*960 25fps raw12, in this module. The Serializer in camera is Max 96705. The Deserializer connected tda4's csi_rx_1 is Max 96722. It uses the capture1 of tda4 by setting in the capture module. We set tda4's csi_laneBandSpeed =CSIRX_LANE_BAND_SPEED_560_TO_640_MBPS, 96722 phy speed set at 0.6G/lane.

    Now, we can see the mipi signal, as the following figure, in output of 96722, but we can't make sure the corrcet of signal, because we don't have enough professional oscilloscope.

    

    Additional, we see some registers' values about CSI_RX_IF Interrupt Events and compare them with another camera module, which can streamOn ok. The values of registers in two camera modules ara same. 

   

    Here, CSI_RX_IF_VBUS2APB_ERROR_IRQS is 0x0, CSI_RX_IF_VBUS2APB_ERROR_IRQS_MASK_CFG is 0x0xf03b1. 

    Accept your help!

    Thanks!