Other Parts Discussed in Thread: MMWAVEICBOOST, , AWR6843AOP
Hello,
My customer use IWR6843AOP on their customer board. The mmWave SDK 3.5 out-of-box demo works fine on it. They want to run the "68xx Vital Signs" from the Industrial SDK 4.12.0. Flashing works fine. Then sending the CLI commands through the terminal works fine (each command is acknowledged with a "Done") until sensorStart is sent, then the radar responds with an "MSS Exception: ../mss/mss_main.c, line 635."
The CLI commands and acknowledgments go through the CFG port with a terminal application, and the DATA (mss_logger, 921.600 b/s) port is monitored with another terminal application. No data come out from the latter at any time with the vital signs lab. Customer has followed this post and that one ("calibDcRangeSig -1 0 -5 8 256" is used).
Could you please point at what we are missing there?
Thank you.
Best regards,
François.