This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Is there any problem if the TX1~3 and RX1~4 pin is dropped to GND?

Part Number: IWR6843

Hello.

We are designing the module with antenna and IWR6843.

I'm considering the structure of the antenna,the antenna terminal may be dropped to GND by DC.

So Is there any problem if the TX1~3 and RX1~4 pin of IW6843 is dropped to GND by DC?

Best Regards,

T.Murakami.