This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Short range setup error

Part Number: AWR1443BOOST

Hi Team,

The customer would like to set the maximum range of the EVM to 3m.

Suggested that the customer refers to these links: Programming Chirp Parameters in TI Radar Devices and mmWave Sensing Estimator.

They are able to create a new configuration but are receiving the error below:

I checked their ".cfg" file and found a "dfeDataOutputMode 1" included. Can you help further? Please see the files attached for the configurations:

6811.config.zip

I really appreciate any help you can provide.

Regards,

Marvin

  • Hi,

    Can you please ask the customer to start with following config provided in the SDK.

    C:\ti\mmwave_sdk_02_01_00_04_original\packages\ti\demo\xwr14xx\mmw\profiles\profile_2d.cfg

    Please run first this configuration because it has been tested.

    After that please make the changes needed to match the final configuration

    thank you

    Cesar