Hello,
My team and I are trying to verify that our application meets an FCC radar output power requirement and have a few questions. Specifically 3.2.2 in this TI document:
https://www.ti.com/lit/an/spracp3c/spracp3c.pdf?ts=1665498950691&ref_url=https%253A%252F%252Fwww.google.com%252F
Device datasheet: https://www.ti.com/lit/ds/symlink/iwr6843aop.pdf?ts=1667490529439
1. Is the single transmitter output power EIRP of 15 dBm out of the chip package or out of the antenna?
2. If multiple transmitters are energized at the same time, how does that factor into our calculations?
3. The formula for power density in the reference document defines R as the minimum separation distance. Is that the separation from the energy source to the target? Section 3.1.2
4. Does distance to the target factor into the average and peak TX power requirements listed in section 3.2.2?
5. A software teammate received advice from TI about setting the output power to 10. The suggestion was to set register 'txOutPowerBackoffCode' to 0x0A0A0A, with the intention of setting each antenna to 10 dB (0x0A). I am confused by that since the documentation refers to this setting as a backoff, "how much the transmit power should be reduced from the maximum". Thus, a setting of 0x0A would not set the power to 10, but set the power to (max - 10). Can you clarify?
Thank you!
Jeff
Norbert Health