Hi team,
Here's an issue from the customer may need your help:
D:\zj\AutomotiveToolbox\mmwave_industrial_toolbox_4_1_0\labs\people_counting\68xx_3D_people_counting is used.
Int32_t DPU_radarprocess_process on DSS side (Void *handle, cplx16_t * pDataIn, void * pDataOut, Int32_t *errCode), where pDataIn is the address of the radarcube. The address is 0x20000000.
However, on the MSS side, static Int32_t rangeProcHWA_ConfigEDMA_DataOut_nonInterleave, One variable in this function is syncABCfg.destAddress= (UINT32_t)rangeProcObj->radarCubebuf; The address is 0x51000000.
Why is the starting address of the radarcube at a different core? Could you help check this case? Thanks.
Best Regards,
Cherry