Hi team,
Customer has THREE questions, please help to solve the problem
1)I downloaded the ultra librarian CAD/CAE symbol frome below link for AWR2243ABGABLQ1 for Altium with Functional Symbol Pin Ordering and after review, I found 3 errors when validating signal names in the symbol vs the datasheet.
vendor.ultralibrarian.com/.../
P4,R3 was labeled as Reserved but should be I2C_SCL and I2C_SDA respectively
R7 was SPI_CS_1_N should be SPI_CS_1.
Please verify and update symbol as needed.
2)Also in the evaluation schematic, it looks like a different version of the symbol is used and R7 in this version is correct but P4 and R3 still show reserved but are connected to SCL and SDA respectively. Also, P12 should be NRESET, pin name is incorrectly should as RESET but net lable does correctly reflect NRST.
There's also mismatches within the datasheet HS_Debug signal names. Example HS_M_Debug1 (used in Ultra Librarian symbol) vs HS_Debug1_M (used in evaluation schematic)
Table 8.1 TX1-4 should be TX1-3
3) Pins that appear to be multifunctional but are not clearly identified as such.

Could you help?
Thanks & Regards,
Jiahui