Hi,
I am using txOutPower to decrease out power of Tx antennas, here is the related configuration:

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am using txOutPower to decrease out power of Tx antennas, here is the related configuration:
Hello.
The TX output power back-off code is 1) not in dB and 2) in decimal notation but from a converted hex number. It is a 24 bit value, with every 8 bits representing the TX backoff for each transmitter. For example, for a 10 dB back off for all 3 transmitters, the hex number would be 0A0A0A, which then converted to decimal is 657930. You can do the same with 30 dB as well. As a result, putting 30 as the parameter value in profileCfg is very close to 0 dB backoff, which is why you are still getting the detected points.
Hope this helps,
Santosh
Hello Jun.
The power on that scale is relative so you won't see a major drop off even with a reduction in transmit power. Also, why are you not trying to detect points?
Sincerely,
Santosh