This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Maximum Pulse Repetition Frequency

Part Number: IWR6843ISK-ODS


Hi,

Good Day.

What is the maximum PRF (Pulse Repetition Frequency) for the IWR6843ISK-ODS?

Please advise. Thank you very much.

Best Regards,

Ray Vincent

  • Hello.

    Pulse Repetition Frequency is not a term we typically use to describe the speed at which pulses are sent; we refer to the individual pulses as chirps and you can have certain number of chirps in a frame.  You can also specify a time length for the frame.  We have a tool called the sensing estimator which can be used to determine how many chirps can be sent per frame, which can then give you the same information as the PRF.  I have included a link here.  With regards to the maximum that this can be, this all depends on a variety of configuration settings and the sensing estimator can help you figure out when you have hit the max for a specific configuration.

    Hope this helps,

    Santosh