Other Parts Discussed in Thread: AWR1843
I have a question about AWR1843Boost.
Is there a fixed transmission range for the antennas Tx1, Tx2, and Tx3 of the installed transmitter?
Tx1 and Tx2: Azimuth antenna
Tx3: Antenna for elevation angle
As far as the following sentences (SDK User Guide) are concerned, I judged that the antennas are divided into azimuth and elevation antennas.
The azimuth and elevation antennas can both be enabled using bitmask 0x7 (i.e. tx1, tx2 and tx3).
For example, in xWR1642BOOST, the 2 azimuth antennas can be enabled using bitmask 0x3 (i.e. tx1 and tx2).