This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: area scanner

Part Number: AWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH, AWR1443

Hi,
I have the AWR1443Boost silicon revision 3.0.

I need to connect the radar to the pelvis of a subject and scan the environment during its ambulatory motion.

To have a first test run with the radar I was able to flash the demo binary file to the board (SDK version 2.1) but I am not able to flash anything else (it gives me the error: following binary is not suitable for the board), although I download it precisely for the xwr14xx board).

Which toolbox version do I need?

Additionally, is there any tool that may help me program the correct binary to flash to the device?

I hope I was clear enough.

Thank you kindly,

Max