This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Building OOB demo in CCS under linux fails

Part Number: IWR6843ISK
Other Parts Discussed in Thread: MMWAVEICBOOST

Hello,
I am trying to build the out of box demo by my own in order to adapt the firmware later on.

My Setting is:

OS: Ubuntu 20.04
CCS: 11
MMW SDK: 3.6.0
MMW Industrial: 4.12.0
Mono: 6.12.0.182 

I have set the environment for iwr68xx with the setenv.sh script.

With the commands below the binary is successfully built  (however, I haven't flashed yet)
cd ${MMWAVE_SDK_INSTALL_PATH}/ti/demo/xwr68xx/mmw
make clean
make all

But when I want to build the demo in CCS, building the DSS works fine but when I want to build the MSS, the auto-generated makefile contains .exe programs which of course fails on a linux machine (except for out2rprc with mono). However flags in the Arm linker seem to look okay. I am aware of the Image_Creator_User_Guide but building with CCS it seems to follow the exact same steps and doing it manually shouldn't be the only solution.

My Questions:

1. How can I successfully build the out of box demo in CCS? My procedure was to first rebuild the DSS and then rebuild the MSS.

1. I noticed that In CCS I can only configure the build as "Debug". Does this build (ones it builds successfully) also work without the MMWAVEICBOOST carrier card?

Thank you