Other Parts Discussed in Thread: AWR1843
Hello,
Below is the details of testing:
board: AWR1843 AOP EVM
Obstacle: Mild steel (sheet 3mm thick) Cube of dimension 40x40x40cm
Lab package: Obstacle detection
We tried to use the above cube as obstacle for testing and observed that when cube is not detected at all places(FOV beyond +-30 degree).Here's the default configuration we used:-
SensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 0 1 1
profileCfg 0 77 7 7 58.0 0 0 67.978 1 256 5020 0 0 36
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 16 0 100 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 1 4 12 4 2 8 2 350 30 2 0 5 50 0.5
dbscanCfg 4 4 13 20 3 256
sensorStart
Hence decided to lower the CFAR threshold for improved detection.
Then we modified config as below:
cfarCfg 1 4 12 4 2 8 2 80 30 2 0 5 50 0.5
Now We are able to detect cube at all locations but we observed few ghost points interfering with actual target cube.
We have below questions.
1.Are there any other parameters in the configurations to improve the detection suppressing ghost points.
2.What is the CFAR threshold relation between obstacle detection and OOB with an equivalent example (because in OOB its mentioned in DB and in obstacle detection its in linear).
3.How to decrease the Max-range of the radar, I tried increasing the frequency slope as per the formula but the GUI hanged.(This was to avoid any reflection we got from wall).