Other Parts Discussed in Thread: MSP-EXP430F5529LP, TUSS4470, TDC7201, TDC7200, TDC1000
I have two BOOSTXL-TUSS4470 I need to link these to be master and slave, as to take a ToF measurement between PMMA transducers?
The manual says:
3.5.2.5.3 External Sync and Trigger To synchronize the time-of-flight command with an external system or another TUSS44x0 EVM, use the external sync and trigger run feature. When the En checkbox is checked, the GUI/EVM becomes a syncslave, where BOOSTXL-TUSS44x0 pin-11 monitors for a low-to-high transition. The Master checkbox enables the GUI/EVM to act as the sync-master, such that the MSP-EXP430F5529LP forces a low-to-high transition on BOOSTXL-TUSS44x0's pin-13 when the START button is clicked in the Run Options group.
How do I link two TUSS4470s together?
Kind regards
Ben