Device: AWR2243
Architecture: Cascade
Issue: How to switch off the amplifiers not in use while one of the TX is "chirping"
Example: TXs number= m TXn on (Chirp ongoing) TX1, TX2, ....;TXn-1, TXn+1.....TXm Off
Aim: To reduce as much as possible the unwanted signal from the TXs that are not "chirping"
Questions:
(1) Is it possible to completely switch off the TXs are not working while one (only) TX is chirping?
(2) In case yes: How much time the switch on/off procedure takes?
(3) Wich is the signal suppression (dBc) relevant to the TX is forced to off ? (Example: TX On >> Pout=13 dBm TXoff >> Pout = -40 dBm Suppression = 53 dBc)
Please advise us the best way to achieve the faster on/off cycle along with the better signal suppression
Thanks
Luigi