Dear Expert.
I am using AWR2243 in a multichip cascading structure with dozens of AWR2243.
-
What is the isolation (in dB) between each TX channel?
for example, If TX1 transmits chirp at full power 13dBm, how much power is transmitted over the other two transmitters (TX2, TX3).
-
The transmitting power for each of the TX channels (TX1, TX2 and TX3) will be controlled via the register (CHIRP_TX_EN 0x0101 - AWR_CHIRP_CONF_SET_SB). Do you think this is the right approach?