Other Parts Discussed in Thread: DCA1000EVM,
Hi, Ti
When I use the Long Range People Detection Demo(dev.ti.com/.../node, there are some questions:
1. Why is the beamwidth 22.5 degrees, can we modify the beamwidth, and if so, how is the beamwidth modified?
2. If the beamwidth is 22.5 degrees and the azimuth is 0 degrees and the perceived range is 7 meters, then the perceived FOV is [-11.25°, +11.25°]? That is to say, it will not be disturbed by moving targets other than FOV?
3. I use IWR6843ISK+DCA1000EVM hardware and the config file "6843_100m_2D_advanced.cfg", we only modify the following configuration to collect data. We set the data collection time to 30 seconds, but actually only 6 seconds of data can be collected. By calculation I think the parameter setting requirements are met, but it doesn't seem to work properly. May I know what is the reason?
Thank you very much!