Other Parts Discussed in Thread: USB2ANY
After installed the PGA970EVM GUI software, I got a strange issue never discriped in the software user's guide.
In the GUI, only <FRAM & DEVRAM> <Data & Waveform RAM> item can work.
Other items show as <Interface Settings [Broken] > <ADC Settings [Broken] > with red backgrand.
Is there any wrong settings when I installed the software , or should I download any firmware into the PGA970chip first?
USB2Any firmware already updated ;
The short jumper J11 J12 J18 J19 installed and J15 connect 1-2;
The Voltage 12V 7.5V 5V 3.3V AVDD 3.0V and DVDD1.86V ,all checked.