This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: I can't use 3 TX with advFrameCfg

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843AOP

Hello,

I want to send a configuration to my radar with 2 profiles and 3 TX per profile. Like this:

 :

So I send in the demo 

However I have an error message:

Please see errors in the Consoles on Configure Tab. Error: Incorrect config reported by target. Hint : Change configuration and try again

And when I look at the console:

mmwDemo:/>sensorStart

Error -1

 

I don't understand why, especially since my configuration works very well if I use only 2 TX like this: 

I can also make my radar work with 3 TX if I don't use advFrameCfg like this:

Here are my two complete .cfg if ever.

profile_advanced_subframe_2TX.cfg

profile_advanced_subframe_3TX.cfg

frameCfg_3TX.cfg

If you have an idea I'm interested!

thank you in advance

Dimitri