This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: Timestamp on MMWCAS-RF-EVM

Part Number: MMWCAS-RF-EVM
Other Parts Discussed in Thread: MMWCAS-DSP-EVM, , AWR2243, AWR1843

Hi Team, seeking some information for a customer. 

Have acquired several MMWCAS-RF-EVM and MMWCAS-DSP-EVM. We want to synchronize the data captured with the radar with other sensors. In order to do that, we need to timestamp the frames stored in the SSD of the MMWCAS-DSP-EVM. I have a few questions I hope you can answer regarding this issue:

  1. Is there any firmware that adds the timestamp to the frame?
  2. Can you provide the firmware running on the MMWCAS-RF-EVM before compiling? We have found the code for the old AWR1843 and modified it to include the timestamp, but we could not find the source code for the large board. (We understand the large board are four cascaded AWR2243 chirps, but the default firmware we load with the mmwavestudio is only provided in the compiled version)

 Thank you.

-Mark