I am working on a prototype using the TUSS4440 sensor paired with a Pro-wave 235kHz transducer (xfrmr driven using a fixed Wurth xfrmr). When I test this transducer and transformer with the EVM I get excellent minimum distance performance ~2-3inches from the sensor face. With my board layout using the same parts, I see a minimum sensing distance of 4-6inches, which is a problem for my application.
What steps can I take to improve minimum sensing distance and why do you think I am seeing this difference? I am using the same tuning network / xfrmr / xducer / parameters etc.