Hi,
Good Day.
The customer is contacting us to ask about our single-point temperature-sensing products. They have a test apparatus that has a 1/2” (inside diameter), single-ply silicone hose that has SAE-10 mineral flowing through it at (approximately) 120*C. The measured flow rate range is: 1.5 L/Min to 9 L/Min
They have tried the “Traceable Digital Thermometer” which is thermistor-based, accurate to three decimal places, and able to point measure a flowing fluid’s bulk temperature between 50*C to 150*C. It originally was made by Cole-Parmer. The software that enables the probe’s monitor to communicate with a computer is old and does not work at all. Hopefully, we have something else for them that meets their temperature sensing and measurement requirements.
Please advise. Thank you very much.
Best Regards,
Ray Vincent