This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Can the CLI package be used with the SPI Bus

Part Number: IWR6843AOP

Looking at the code for the CLI package in the mmwave SDK 3.06 I see that it is setup for a UART connection. The documentation does not suggest I can easily set the CLI to accept data via the SPI bus. My question, is there a simple change I can make to use SPI bus comms rather than the UART connection or will i have to write my own version of this?