Hello,
I have designed a custom board with AWR1843. I connected the Vout_PA pins to the VIN_RF2 as shown in the evaluation board. I am supplying 1V to the VIN_RF1 and VIN_RF2 pins from an extarnal LDO just like the evaluation board. My concern is when I turn the device on for the first time what will be the default configuration for the RFLDO BYPASS_EN bits. I understand from the Interface Control Document, I am supposed to set them as 1, 1 to bypass the LDO and disable the PA_LDO. I am concerned if they start up on the wrong setting it may damage the board.
- What are the default configurations for the RFLDO BYPASS_EN bits?
- If they are set as 0 on start-up, how should I power the device for the first time to flash the memory?
- When the board starts up in SOP mode set for flashing what is the behavior of the LDO?
Thanks in advance, hope my questions were clear.