Hello,
I'm wondering how I'm correctly calculate the distance to far field in TDM MIMO Mode. Do I consider a single antenna patch as aperture since there is only one TX-antenna active at time or
do I have to consider the whole 86 virtual antennas?
1. Single Antenna:
D = ca. 4 mm
Rff = 2 * D ^ 2/lambda = ca. 8 mm
2. Whole virtual antenna array:
D = 85 * lambda/2 = 165 mm
Rff = 2 * D ^ 2/lambda = ca. 13 m
Second Question: Are there any known drawbacks working in near field with this evaluation board?
Thanks,
M. Mueller