Hi,
Does the SDK Demo MSS enables the use of hardware trigger using the GPIOs? If not how can I add support for this feature?
Thanks
Yuval
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Does the SDK Demo MSS enables the use of hardware trigger using the GPIOs? If not how can I add support for this feature?
Thanks
Yuval
Hello Yuval,
There is no provision to directly use the hardware trigger.
To read more about this feature you will have to go through the interface control document, which is available if you download the dfp package 1.2.6.3.
Then you can go to the C:\ti\mmwave_dfp_01_02_06_03\docs\mmWave-Radar-Interface-Control.pdf
Ther you can go the section 5.5.3 Sub block 0x0102 – AWR_FRAME_CONF_SET_SB, if you go to page 85, 86 it explains how the pulse should be configured.
Then you will need to maintain the sync time with the GPIO (initialize this GPIO using the driver) using a timer in the Application code and this is how you will be able to trigger the frame externally.
Adding the picture from the interface control document for reference:
Regards,
Saswat Kumar