This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: Sensing Estimator Tool

Part Number: AWR1843AOPEVM


Hi,

1.) I am trying to set mmwave parameters using Sensing Estimator tool. However, there are two different tools under the same name. One of them is that calculate the appropriate chirp and frame parameters, if give to the max. range and velocity, range and velocity resolution. Here is the link:

dev.ti.com/.../

Other one is that calculate the max. range and velocity, range and velocity resolution, if give to chirp and frame parameters. Here is the link : 

https://dev.ti.com/gallery/view/mmwave/mmWaveSensingEstimator/ver/2.0.0/

However, these tools are not giving the same results. The values of  some calculated parameters don't match.   

Which tool should I use for calculations? Are there any restrictions on the tools?

2.) I'm trying to run the sensor using hard coded in CCS. However, I enter the calculated parameters in the tools, I get an error. This error is about subframe periodicity. Even though I entered the appropriate range value for parameters, I get exception in the debug mode. I realized that if under 20 ms periodicity causes exception. Is there any restriction for this parameters?

Thank you.

  • Hi,

    Use sensing estimator 2.0. This is the most updated version. Can you also tell us what parameters you put in and what results are different?

    2.) I'm trying to run the sensor using hard coded in CCS. However, I enter the calculated parameters in the tools, I get an error. This error is about subframe periodicity. Even though I entered the appropriate range value for parameters, I get exception in the debug mode. I realized that if under 20 ms periodicity causes exception. Is there any restriction for this parameters?

    Please open another thread for different questions. This helps us keep the forum organized and searchable. Thank you.

    Best,

    Nate