Hi Team,
My customer is going to use our TMP117 in their peoject.
They have below questions need your kindly comment.
- For below averages sampling, we should understood that the temperature will be detected one time every second, and 8 times will be sampled for averaging in one data? and the sampling time for each time is 15.5ms?
- Is below consumption current in red box what I highlight is workable for Question 1's sampling method ?
At this time, the I2C should transmit data to the MCU. The I2C bus should be active, right?
Can you provide 8 average mode on + serial bus active power consumption for customer ? - If we set to detect the temperature one time per every minute, 8 average mode on, can the current consumption be calculated as follows ? If it is not correct, can you guide how to calculate it ?
[(15.5ms x 8 x 135uA)+(59.876sec x 1.25uA)] / 60sec= 1.526uA
Thanks!
Kai