This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Performance Measurement for MMWave devices

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR1443, IWR6843AOP

Hello,

I'm looking to improve the frame rate and add a few features to the Water/Ground demo. I got it working on the IWR1443, and am looking to port it to the IWR6843AOP, and increase the framerate. My only real concern is being able to get a 2-4x speedup on framerate, and was wondering (i) if there is a tool provided to profile the performance, and (ii) how realistic this speedup is.

Thanks!

  • Hello.

    You can speed up the framerate and see its performance by adjusting the frame periodicity in the frameCfg command in the configuration file.  You can find which parameter this is by referencing the SDK user guide for the SDK you are using.

    Sincerely,

    Santosh