This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Question about device compatibility

Part Number: DCA1000EVM
Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843

Hello TI community,

I'm having a very basic question because I'm about to buy a DCA 1000EVM device. i know that it's compatible with IWR 1443 and IWR 1642. But i was wondering if it could be compatible with IWR 6843 because i want to buy one also. I have seen that the IWR 6843 could be mounted over the MMWAVEICBOOST board.

And what is the difference between the two (using the DCA 1000 and the MMWAVEICBOOST Board).

Thank you in advance.

Have a good day.

Abdellah.