This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: OSC_CLOCKOUT

Part Number: IWR6843
Other Parts Discussed in Thread: MMWCAS-RF-EVM

In the data sheets on page 12 (AOP version), it is said:Reference clock output from clocking sub system after clean up PLL

In the Fig 9-2 on page 60  (AOP version) output is taken between XO/slicer and clean up PLL. So, there is a contradiction.

I suppose you can't design a massive mimo radar with IWR6843 chips because you would need to get the same 20 GHz signal for the chips, as in MMWCAS-RF-EVM with AWRx chips.

Is there or is there going to be a way to generate massive mimo radar at 60GHz frequency range with TI circuits?

Regrds, Jarmo Kivinen