This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP468: Logic High value

Part Number: TMP468

Hi,

For doing a DC analysis, Can i get the VOH min value for TMP468

  • Hi,

    All the digital output pins on the TMP468 (SDA, THERM1, THERM2) are open-drain and can only drive the pins low, so there is no specification for VOH. These pins require a pullup resistor to a voltage between 1.7 V and 3.6 V.

    Best regards,

    Jesse