Hi
I am interested in using the LMP91000. We have our existing design, but we would prefer to send it via a secure link or email, so it's not available in the public domain.
We intend to use this for NO2,NO and OX sensors. Before I get into technical questions, I would like to know the following.
Please find attached the following:
- Our Existing design(to be sent via email if possilbe) uses the NO2 and OX Sensor.
2. We are using the ISB board from the NO sensor manufacturer. This PCB is similar to our custom board but is configured slightly differently to bias polarity.
3. Data Sheets For N02, No, and OX Sensors
These Sensors output a WE and Aux Voltage output. When used with LMP91000 I guess we can simply monitor WE signal only and ignore the Aux.
If I have understood the datasheet correctly, LMP91000 only output an Analogue signal?
Would this LMP91000 be adequate for these sensor types?