Other Parts Discussed in Thread: TMCS1107,
Hi ,
I have a TMCS1107A1BQDRQ1 Hall Effect Sensor from TI, a single phase AC power supply and an AC load. I want to measure the current on the AC line by using the schematics given below, but I couldn't. The sensor's voltage output is always 2.5V regardless of the current drawn by the AC load or the reference voltage. I also tried to measure the current both in high side and low side of the circuit but nothing has changed.
To verify the sensor and the board, I used a DC supply and a DC load and it worked as expected.
What am I missing? Can TMCS1107A1BQDRQ1 be used in both AC and DC applications? If this is the case then what is wrong with my circuit?
Thanks in advance,