This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Reason why 1.4 V is not output from VOUT_14SYNTH

Part Number: AWR1843


I tried powering the AWR1843 and the voltage coming out of VOUT_14SYNTH was 0.9 V.
What are the possible causes when this value is printed?

The wiring diagram is as follows.
I am inputting a voltage of 1.8 V. (The capacitor is also connected in the same way as AWR1843.)