This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: Flash Memory Gets Deleted Completely

Part Number: AWR1843BOOST


Hello E2E Experts,

Good day.

1. Which writes calibration data onto the flash memory.

2. Runs on the field which restores the calibration data from flash(non-volatile memory) during boot time.

However, when I flash the application which runs on the field, the entire non-volatile memory gets erased which results in the deletion of calibration data. My application size is 228 K bytes only!. I have chosen 0xA0000 as a starting location in non-volatile memory to store calibration data that is greater than 228Kbytes.

 Could you please help me why the entire flash memory gets erased if I upload the image? This is not the case with ccsdebug image.

Thank you in advance.

Regards,

CSC