Other Parts Discussed in Thread: FDC1004
Hi Ti Support Team,
My name is Xinghao. I am a graduate student from the University of Southern California. I am currently using the FDC1004QEVM board to measure multiple capacitive strain sensors. However, I noticed there is a big difference between the capacitance measured by this board and our lab's LCR meter. For example, I tested a 2 pF +/0.25pF ceramic capacitor, I got 2.19 pF on my LCR meter at 20kHz frequency. But for FDC1004, I got around 8 pF for single ended measurement after connecting SHIELD 1 on my coaxial cables (the sensor's two ends are connected to CIN1 and GND). I also tried differential measurement by connecting one end of my sensor to CIN1 and taking CIN1-CIN2, and it gave me about 4 pF. It seems I still need to remove more parasitic capacitance because the manual says this board actually measures anything between the sensor and ground. In addition, CIN1 and CIN2 are probably interfering each other, but I am not too sure. Can you help me on this?
Thank you very much.
Best,
Xinghao