Hello, I saw AWR1843 and thought, is it correct to understand that Tx1 and Tx3 only deal with Azimuth direction, and Tx2 corresponds to Elevation direction?
(If you have any materials describing the roles, please let me know.)
I made this decision for two reasons.
1.The resolution of Azimuth was 14.5 deg.
This is the same value calculated with only two transmit antennas.
2. On page 14 of the PDF below, only the plane is applicable to the transmitting antenna, and I have determined that the same specifications are used for AWR1843.Millimeter Wave (mmw) Demo for XWR16XX.pdf