Hello Experts,
I am currently using IWR6843ISK EVM board and using Area Scanner and People Counting labs. I want to implement my test set up in a small room for the Radar sensors by fixing them to the wall. I have few queries in modifying the .cfg files.
Currently, I am using two labs for my data extraction. I want to test these two labs and get the localization of the objects and humans.
For object data Localization: I am using Area scanner lab with this below CFG configuration: area_scanner_68xx_ISK.cfg
|
For Human data Localization: I am using 3D people counting lab with this below CFG configuration: ISK_6m_default.cfg
ISK_6m_default.cfg from 3D people coutning lab |
|
Query 1 : Could someone please give which of the Parameters from the CFG file are responsible to update:
- The field of view value to 60 Degree azimuth and 60 deg elevation?
- Change the Range of the Radar sensor to 2.5 meters
I have referred the MM wave SDK user guide and people counting Track layer and detection layer user guides, but it is not clear to understand which parameters in the CFG file are responsible to change the Field of the view of the sensor and range ?
Query 2: What is the process of updating the CFG files? Is it like changing the CFG file in a notepad would work ?
Looking forward to your reply!
Best Regards,
Shravya