This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: HWTRIGGER for both master and slave devices

Part Number: AWR2243


Hi,

In swra574b section 5.5, it says, "It is possible to trigger all AWR2243 devices (including the master) in HWTRIGGER mode. For this, the host needs to generate DIG_SYNC_IN pulses of the right periodicity and feed to DIG_SYNC_IN pins of all the chips (including the master)".

My questions are:

1. Is it possible to share the same signal from the host processor to DIG_SYNC_IN of both master and slave?

2. Where can I find information on timing of DIG_SYNC_IN signal for master and slaves?

Thanks,

Santhosh