This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Is 'dynamic per-chirp Tx phase-shifter' functionality supported in cascade, continuous mode, configuration?

Part Number: AWR2243

Hi,

Could it be confirmed that, 'dynamic per-chirp Tx phase-shifter' functionality (AWR_DYN_PERCHIRP_PHASESHIFTER_CONF_SB), is supported in AWR2243 cascade (4 devices, continuous mode) operation?

We don't think there is anything to suggest that it isn't supported, from reading through the Interface Control Documentation, we just want to be as sure as possible, before investing in design and test based upon it.

We're assuming that once in cascade operation, each device can be provisioned with dynamic configuration commands in isolation, as they would be as standalone devices, and hold the same requirements for timings etc.

Kind regards,

Mike