This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: bpmconfig with HVAC binary

Part Number: IWR6843ISK


Hi Team,

Can you please help with the inquiry below?

Hardware setup: 6843ISK
Industrial tool box: 4_11_0

Binary: Prebuilt binary sense_and_direct_68xx_lab.bin

 I have created my own config file and was trying to use the bpmconfig command (also modifying the chirpconfig). The exact config file is as follows:

sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg 0 1 1 1 
profileCfg 0 60 97 7 20.82 0 0 60 1 160 12499 0 0 158
chirpCfg 0 0 0 0 0 0 0 5
chirpCfg 1 1 0 0 0 0 0 5
frameCfg 0 1 16 0 50 1 0
lowPower 0 0
guiMonitor 1 1 1 1
cfarCfg 6 4 4 4 4 8 12 4 8 50 63 0
doaCfg 600 666 30 1 1 1 300 4 2
AllocationParam 300 800 0.1 30 0.5 20
GatingParam 3 1.5 1.5 0
StateParam 3 3 10 40 5 600
SceneryParam -5 5 0.25 10
FilterParam 2.0 0.5 1.5
trackingCfg 1 2 300 15 67 105 50 90
classifierCfg 1 1 3 500 0.8 1.0 0.95 10
bpmCfg -1 1 0 1
sensorStart

However i get a message that bpmCfg is not supported. I tried flashing the binary file again but continue to get the error message.

What can i do to enable the bpmCfg?

Essentially, i want to increase the power, hopefully improving the SNR and range.

Thank you.

Regards,

Marvin