This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432: Questions about memory replacement materials

Part Number: IWRL6432


  1. May I ask if the IWRL6432 EVM recognizes the flash as MX25V1635FZNI (6x5mm WSON8), can I use MX25V1635FZUI (2x3mm USON8) instead?
  2. The VDD range of MX25V1635F is 2.5V~3.6V. Do you have a 1.8V memory that you can recommend?