Other Parts Discussed in Thread: AWR6843
Hi,
I own a AWR6843AOPEVM device and would like to run this example or this one.
The thing is that I would like to avoid using a PC for processing. The ideal scenario for me would be to flash an external device with all that's needed for processing, such as Raspberry Pi.
Moreover, in the second example I've mentioned above, it says:
Note: In this version, the AWR6843 outputs the spherical-coordinate point cloud. Zone mapping and decision state machine processing are perform for the short term in Matlab. These will be moved to the xWR6843 in a near term release to the mmWave Automotive Toolbox.
Is it already done? Where can I find that release?
In the first example I've mentioned above, which seems more up-to-date, such a release isn't mentioned and the use of MATLAB still exists.
If there isn't such a release, I'd like to know if it's possible to use a sort of a compiler to do that myself. Is there a specific one that is recommended? What would be the process of implementing that?
I would appreciate some help with that,
Thanks.