Part Number: LDC1612
Other Parts Discussed in Thread: LDCCOILEVM,
Hello,
I am utilizing a LDC1612 with a F28379D launchpad to measure lateral movement on coil B from the LDCCOILEVM. Yesterday, I was able to create a 1mm resolution scale used from LDC data from 0mm to 59mm. To create this scale, I divided DATA0 by 1000 and mapped mm points along the coil with a ruler. With this data collected, I was able to create a linear equation that was included in the code. I power cycled the system a few times to see if the scale was usable, and in fact it was. After 24 hours however, I noticed that the scale does not work. Yesterday’s 0mm data point was 7403, and today’s 0mm data point is 7484, leading to a offset of 81. I included this offset in the code today, however the scale is not as reliable. I was wondering what could lead to this variation in data. The hardware system/ target has not changed. The only change in software is the subtraction of the offset. Below are the system parameters:
Coil B from LDCCOILEVM with 820pF capacitor connected to LDC1612 portion of LDC1612EVM.
100mm x 25 mm meta target.
Launchpad is utilizing a 400k i2c clock.
Register values for LDC1612:
RCOUNT0: 0xFFFF
RCOUNT1: 0x0009
SETTLECOUNT0: 0x0012
SETTLECOUNT1: 0x0001
CLOCKDIV1/2: 0x1001
ERRORCONFIG: 0x0001
DRIVECURRENT0/1: 0xF000
MUXCONFIG: 0x820C
DEVICECONFIG: 0x1E01
Thank you.